Software Version 2.14.0

Create Application Items for Measurement in Dimmer

You can quickly create the required C-Bus application items for the project based on the current configuration of the Measurement category in a C-Bus Dimmer.

To create application items:

Pre-requiste: The Create Application Item button is enabled only if the Device ID is assigned.

  1. Select Dimmer device >Measurement >click Create Application Items.

    NOTE: The Application Items field is displayed only when a project C-Bus Dimmer device is loaded into the Property Editor.

    The Create Application Items dialogue box appears.

    By default, the Measurement Channels for Lamp Run Time and Channel Temperature for Used Dimmer Channels and Measurement Channels for C-Bus Power Supply Current, C-Bus Power Supply Voltage and Unit Temperature check boxes are selected.

  2. If you assign values for Send Trigger Group or Clear Trigger Group in Measurement section of PROPERTIES, then the below check boxes are selected in Create Application Items dialogue box:

    • Trigger Group Action Selector for each Used Dimmer Channel (Lamp Run Time and Channel Temperature)

    • Trigger Group Action Selectors for C-Bus Power Supply Current, C-Bus Power Supply Voltage and Unit Temperature

    • Trigger Group Action Selector 255 for all measurements

    Measurement in PROPERTIES

    Create Application Items

  3. Click Create to generate the application items. C-Gate creates the items and displays them in the relevant application workspace in the client, based on the NCC Dimmer_Create Application Items file in the project folder.

    NOTE: Below are the creation conditions:
    • Creation occurs only when the associated Application Item check box is selected.

    • If the Measurement Application is not present on the C-Bus network, clicking Create Application Items adds the Measurement Application to the network before beginning the creation process.

    • Success message appears.

      The below image displays the assigned Trigger Group in the Trigger Application.

      The below image displays the assigned measurement channels in the Measurement Application.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.