SENPIRIC (5754ODPE)
The 5754ODPE is a 360-degree, surface-mounted Passive Infrared (PIR) occupancy and light level sensor designed for indoor use. It forms part of the C-Bus control and management system and automates lighting by detecting occupancy and measuring ambient light levels to activate connected loads or scenes.
To configure the field informations of PROPERTIES in SpaceLogic C-Bus SENPIRIC sensor, refer SENPIRIB (5753L) Sensor.
-
An Information pop-up appears.
-
Click OK to proceed.
-
Block field is disabled if Function is set to Unused / Light Level & Sunset Adjust / Occupancy Sensitivity Adjust.
-
Block field is enabled only when Function is set to Block Timer Adjust.
-
When Block Timer Adjust is assigned to Function in Potentiometer A, the same option is excluded from the Function drop-down list in Potentiometer B and vice versa.
-
When Occupancy Sensitivity Adjust is assigned to Function in Potentiometer A, the same option is excluded from the Function drop-down list in Potentiometer B and vice versa.