Advanced Configuration SENPIRIC
-
Click Advanced Configuration in the Configuration section of PROPERTIES.
The Advanced Configuration SENPIRIC dialogue box appears. -
For more information on configurations in the Advanced Configuration, refer Advanced Configuration SENPIRIB.
-
The key difference between the SENPIRIB and SENPIRIC models lies in the number of potentiometers on the device.
-
SENPIRIB : Potentiometer (A)
-
SENPIRIC : Potentiometers (A and B)
-
-
When you select Light Level & Sunset Adjust function from Potentiometer (A) and Potentiometer (B) section, using the Function drop-down list, they allow external control of light level maintenance.
An Information pop-up appears.
-
Click OK to proceed.
Potentiometer
Description
A
Sets the desired light level (in lux).
B
Sets the allowable lux range around the light level target.
-
Block field is disabled if Function is set to Unused / Light Level & Sunset Adjust / Occupancy Sensitivity Adjust.
-
Block field is enabled only when Function is set to Block Timer Adjust.
-
When Block Timer Adjust is assigned to Function in Potentiometer A, the same option is excluded from the Function drop-down list in Potentiometer B and vice versa.
-
When Occupancy Sensitivity Adjust is assigned to Function in Potentiometer A, the same option is excluded from the Function drop-down list in Potentiometer B and vice versa.