DOCA0258EN-00

Access to the Monitoring & Control Page

The Monitoring & Control page is displayed:

  • After you connect to the standard web server.

  • When you click Monitoring & Control in the menu headers at any moment during navigation and from any page displayed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?