LTMT Main Unit with EtherNet/IP Protocol
Overview
| NOTICE |
|---|
|
UNAUTHORIZED ETHERNET PORT USAGE
Failure to follow these instructions can result in equipment damage.
|
The LTMT main unit with EtherNet/IP or Modbus TCP/IP communication protocol is equipped with two RJ45 Ethernet ports on the front face. These ports comply with IEEE 802.3 Ethernet standard.
The main physical characteristics of Ethernet ports are:
|
Physical Interface |
Ethernet 10BASE-T/100BASE-T |
|---|---|
|
Connector |
RJ45 |
Description
|
A |
Digital input connectors |
|
B |
RJ45 port for LTMT expansion module connection |
|
C |
RJ45 port for HMI connection |
| D |
RJ45 ports for EtherNet/IP or Modbus TCP/IP communication |
| E |
Device shield ground terminals |
| F |
Temperature input connector |
| G |
Power supply connector |
| H |
QR code to product information page |
| I |
Test/Reset button |
| J |
Status LEDs |
| K |
Digital output connectors |
RJ45 Connector Pinout
The RJ45 wiring layout is:
|
Pin No. |
Signal |
Pair |
Description |
|---|---|---|---|
|
1 |
TD+ |
A |
Transmit + |
|
2 |
TD- |
A |
Transmit – |
|
3 |
RD+ |
B |
Receive + |
|
4 |
Do not connect |
– |
– |
|
5 |
Do not connect |
– |
– |
|
6 |
RD- |
B |
Receive – |
|
7 |
Do not connect |
– |
– |
|
8 |
Do not connect |
– |
– |
Auto-MDIX Interface
Each RJ45 connector on the LTMT main unit Ethernet network port is an MDIX (media-dependent interface crossover) interface. Each connector automatically senses the:
-
Cable type (straight or crossed) plugged into the connector
-
Pin requirements of the device to which the LTMT main unit is connected
Using this information, each connector assigns transmit and receive functions to pin combinations 1 and 2, and 3 and 6 as necessary to communicate with the device on the other end of the cable.