DOCA0258EN-00

Table Format

The TeSys Tera system supports the following Syslog data formats. The data tables have the following columns:

Severity

Version

TimeStamp

HostName

AppName

PROCID

MsgID

SequenceID

Structured Data

Description

Designation

Description

Severity

Indicates the urgency of the message. The values range from 0 (Emergency) to 7 (Debug)

Version

Specifies the version of the Syslog protocol

TimeStamp

Date and time when the message was generated

HostName

Name of the host system generating the log message

AppName

Name of the application generating the log message

PROCID

Process ID of the application that generated the message

MsgID

Unique identifier for the type of message

SequenceID

Additional identifier for the event type

Structured Data

Structured metadata or contextual information about the event

Description

Actual content or message body describing the event

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?