DOCA0258EN-00

Temperature Protection

The table lists the temperature protection of the LTMT main unit.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0ECD (3790)

83 : 01 : 28

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

0

Y

Function setting

0x0ECE (3791)

83 : 01 : 29

RW

0.1

°C

UINT16

250–1800
(step 1)

1300

Y

PT100 pickup*

F

770–3560
(step 1)

0x0ECF (3792)

83 : 01 : 2A

RW

1

Ω

UINT16

2700–4000
(step 1)

2700

Y

PTC pickup

0x0ED0 (3793)

83 : 01 : 2B

RW

1

Ω

UINT16

1600–2300
(step 1)

1600

Y

PTC pickup reset

0x0ED1 (3794)

83 : 01 : 2C

RW

0.1

s

UINT16

1–60000
(step 1)

10

Y

Time delay

0x0ED2 (3795)

83 : 01 : 2D

RW

0.1

°C

UINT16

250–1800
(step 1)

1300

Y

PT100 alarm level*

F

770–3560
(step 1)

0x0ED3 (3796)

83 : 01 : 2E

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0ED4 (3797)

83 : 01 : 2F

RW

0.1

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0ED5 (3798)

83 : 01 : 30

RW

0

UINT16

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?