Analog Input Protection Settings
Description
The TeSys Tera system supports up to four analog inputs with two LTMTAN21 expansion modules.
Each analog input protection settings are made up of eight registers. The order and the description of the settings for analog input 1 are valid for the other analog inputs.|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
Description |
|---|---|---|---|
|
0x0FA0–0x0FA7 (4001–4008) |
84 : 02 : 01 – 84 : 02 : 08 |
RW |
Analog input 1 protection settings |
|
0x0FA8–0x0FAF (4009–4016) |
84 : 02 : 09 – 84 : 02 : 16 |
RW |
Analog input 2 protection settings |
|
0x0FB0–0x0FB7 (4017-4024) |
84 : 02 : 17 – 84 : 02 : 24 |
RW |
Analog input 3 protection settings |
|
0x0FB8–0x0FBF (4025–4032) |
84 : 02 : 25 – 84 : 02 : 32 |
RW |
Analog input 4 protection settings |
Analog Input 1 Protection Settings
The table lists the registers for the analog input protection settings.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0FA0 (4001) |
84 : 02 : 01 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0FA1 (4002) |
84 : 02 : 02 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Detection |
|
0x0FA2 (4003) |
84 : 02 : 03 |
RW |
0.1 |
mA |
UINT16 |
40–200 |
40 |
Y |
Pickup |
|
0x0FA3 (4004) |
84 : 02 : 04 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Time delay |
|
0x0FA4 (4005) |
84 : 02 : 05 |
RW |
0.1 |
mA |
UINT16 |
40–200 |
40 |
Y |
Alarm |
|
0x0FA5 (4006) |
84 : 02 : 06 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0FA6 (4007) |
84 : 02 : 07 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0FA7 (4008) |
84 : 02 : 08 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Diagnostic |