Locked Rotor Protection
The table lists the locked rotor protection for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0DC4 (3525) |
83 : 01 : 19 |
RW |
1 |
– |
UINT16 |
|
2 |
Y |
Function setting |
|
0x0DC5 (3526) |
83 : 01 : 1A |
RW |
1 |
%IFLC |
UINT16 |
150–1000 |
200 |
Y |
Pickup |
|
0x0DC6 (3527) |
83 : 01 : 1B |
RW |
0.1 |
s |
UINT16 |
1–60000 |
100 |
Y |
Time delay |
|
0x0DC7 (3528) |
83 : 01 : 1C |
RW |
1 |
%IFLC |
UINT16 |
150–1000 |
200 |
Y |
Alarm level |
|
0x0DC8 (3529) |
83 : 01 : 1D |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0DC9 (3530) |
83 : 01 : 1E |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto–Reset delay |