DOCA0258EN-00

Installation Rules in a Switchboard

The installation of the LTMT main unit in the withdrawable drawer of a switchboard presents constraints specific to the type of switchboard:

  • For installation of the LTMT main unit in a Schneider Electric Okken switchboard, refer to the Okken Communications Cabling & Wiring Guide (available on request).

  • For installation of the LTMT main unit in a Schneider Electric Blokset switchboard, refer to the Blokset Communications Cabling & Wiring Guide (available on request).

  • For installation of the LTMT main unit in a Model 6 switchboard, refer to the Model 6 Communications Cabling & Wiring Guide (available on request).

  • For installation of the LTMT main unit in other types of switchboard, follow the specific EMC instructions described in this guide and refer to the relative instructions specific to your type of switchboard.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?