DOCA0258EN-00

IP address allowlist

The table lists the IP address for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X Unit

Type

Range Default value

Svd

Description

0x1384 (4997)

88 : 01 : 7A

RW

1

N/A

UINT16

0: Disable

1: Enable

0

Y

IP filter selection

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?