DOCA0258EN-00

Modbus RTU Page Body

The Modbus RTU page contains the following sub-menus:

Level 1 Level 2 Parameter Name
Modbus RTU Statistics* Modbus RTU Frames Received Modbus RTU Frames Received
Modbus RTU Frames Transmitted Modbus RTU Frames Transmitted
Modbus RTU Connections Baud Rate

Baud rate. Possible values:

  • 2400

  • 4800

  • 9600

  • 19200

  • 38400

  • 57600

  • 115200

Parity

Parity. Possible values:

  • None

  • Odd

  • Even

Stop Bits

Stop bits. Possible values:

  • 1

  • 2

Server ID Server ID
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?