DOCA0258EN-00

Overview

The Communication settings page allows you to view or modify the Ethernet configuration, IP configuration, Modbus RTU and field bus protocol settings of the TeSys Tera system.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?