Modbus Enable or Disable Setting
The table lists the Modbus enable or disable settings for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X | Unit |
Type |
Range | Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x13CF (5072) |
88 : 01 : C5 |
RW |
1 |
N/A |
UINT16 |
0: Disable 1: Enable |
1 |
Y |
Modbus HMI Selection |
|
0x13D0 (5073) |
88 : 01 : C6 |
RW |
1 |
N/A |
UINT16 |
0: Disable 1: Enable |
1 |
Y |
Modbus TCP Selection |