DOCA0258EN-00

IP Network Services Page Body

The IP Network Services page contains the following sub-menus:

Level 1 Level 2 Parameter Name
Modbus TCP Port* Port Status Port Status
Opened TCP Connections Opened TCP Connections
Received Messages Received Messages
Transmitted Messages Transmitted Messages
Modbus TCP Port Connections* Modbus TCP port connections. It contains the following parameter values:
  • Remote IP

  • Remote Port

  • Local Port

  • Received Messages

  • Transmitted Messages

  • Sent Errors

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?