DOCA0258EN-00

Definite Time Overcurrent Protection

The table lists the definite time overcurrent protection for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0DCA (3531)

83 : 01 : 1F

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

2

Y

Function setting

0x0DCB (3532)

83 : 01 : 20

RW

1

%IFLC

UINT16

20–1000
(step 1)

110

Y

Pickup

0x0DCC (3533)

83 : 01 : 21

RW

0.1

s

UINT16

1–60000
(step 1)

300

Y

Time delay during motor start (TpS)

0x0DCD (3534)

83 : 01 : 22

RW

0.1

s

UINT16

1–60000
(step 1)

200

Y

Time delay during motor run (TpR)

0x0DCE (3535)

83 : 01 : 23

RW

1

%IFLC

UINT16

20–1000
(step 1)

110

Y

Alarm level

0x0DCF (3536)

83 : 01 : 24

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0DD0 (3537)

83 : 01 : 25

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0DD1 (3538)

83 : 01 : 26

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?