DOCA0258EN-00

Prerequisites

System Requirements

The standard web server operates on the Microsoft Windows® 11 operating system.

Browser Requirements for Using the Interface

The standard web server can be accessed using any of the following supported web browsers.

  • Microsoft Edge Pro version 14 or later.

  • Mozilla Firefox version 13 or later.

  • Google Chrome version 19 or later.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?