DOCA0258EN-00

Overview

The standard web server serves as a remote user interface, enabling you to monitor and control motor operations through a web browser. It provides access to real-time status updates and configuration settings, eliminating the need for physical interaction with the motor. The standard web server supports only one connection at a time.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?