Under Frequency Protection
The table lists the under frequency protection for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0E49 (3658) |
83 : 02 : 21 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0E4A (3659) |
83 : 02 : 22 |
RW |
1 |
%F* |
UINT16 |
90–100 |
94 |
Y |
Pickup |
|
0x0E4B (3660) |
83 : 02 : 23 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
1 |
Y |
Time delay |
|
0x0E4C (3661) |
83 : 02 : 24 |
RW |
1 |
%F* |
UINT16 |
90–100 |
94 |
Y |
Alarm level |
|
0x0E4D (3662) |
83 : 02 : 25 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0E4E (3663) |
83 : 02 : 26 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0E4F (3664) |
83 : 02 : 27 |
– |
– |
– |
– |
– |
– |
– |
Reserved |