Phase Under Current Protection
The table lists the phase under current protection for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0DEE (3567) |
83 : 01 : 43 |
RW |
1 |
– |
UINT16 |
|
1 |
Y |
Function setting |
|
0x0DEF (3568) |
83 : 01 : 44 |
RW |
1 |
%IFLC |
UINT16 |
15–100 |
50 |
Y |
Pickup |
|
0x0DF0 (3569) |
83 : 01 : 45 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
100 |
Y |
Time delay |
|
0x0DF1 (3570) |
83 : 01 : 46 |
RW |
1 |
%IFLC |
UINT16 |
15–100 |
50 |
Y |
Alarm level |
|
0x0DF2 (3571) |
83 : 01 : 47 |
RW |
1 |
– |
BITMAP |
|
8 |
Y |
Reset mode |
|
0x0DF3 (3572) |
83 : 01 : 48 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
50 |
Y |
Auto-Reset delay |
|
0x0DF4 (3573) |
83 : 01 : 49 |
– |
– |
– |
– |
– |
– |
– |
Reserved |