DOCA0258EN-00

Ethernet Network Topologies

Star Topology

A star topology is a network configuration in which all the LTMT main units are directly connected to an Ethernet switch.

Point-to-Point Topology

A point-to-point topology is a network configuration in which the LTMTCUF control operator unit connects the LTMT main unit to the PC.

NOTE: In point-to-point topology, you can also connect the LTMT main unit directly to the PC.

Example of Wiring Diagram

The wiring diagram below indicates how to connect LTMT main units installed in withdrawable drawers to the Ethernet network through the RJ45 connector and hardwired cables.

A

Client (PLC, PC, or communication module) with line terminator

B

Ethernet switch

C

Ethernet shielded cable 490NTW00002 or 490NTW00005 or 490NTW00012

D

Withdrawable drawer part of the auxiliary connector for drawers

E

Fixed part of the auxiliary connector

F

Withdrawable drawer

G

Grounding of the Ethernet cable shield

H

Switch board column

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?