Measurement Data Page Body
The Measurement Data page contains the following sub-menus:
| Level 1 | Level 2 | Parameter Name |
|---|---|---|
| Energy Data | Total Active Energy | Total Active Energy |
| Total Reactive Energy | Total Reactive Energy | |
| Total Apparent Energy | Total Apparent Energy | |
| Frequency | Frequency | |
| Power Factor | Power Factor | |
| Current Phase Sequence | Current Phase Sequence | |
| Voltage Phase Sequence | Voltage Phase Sequence | |
| Current Data | I1 | RMS Current |
| I2 | RMS Current | |
| I3 | RMS Current | |
| Voltage Dta | U12 | RMS Voltage |
| U23 | RMS Voltage | |
| U31 | RMS Voltage | |
| Power Data | Total Active Power | Active Power |
| Total Reactive Power | Reactive Power | |
| Total Apparent Power | Apparent Power | |
| Imbalance Data | Measured Ig | Measured Ig |
| Current Ig | Current Ig | |
| Current Imbalance | Current Imbalance | |
| Voltage Imbalance | Voltage Imbalance | |
| THD Data | L1 Current THD | Phase 1 current total harmonic distortion (THD) |
| L2 Current THD | Phase 2 current total harmonic distortion (THD) | |
| L3 Current THD | Phase 3 current total harmonic distortion (THD) | |
| Voltage THD Data | L1–L2 Voltage THD / L1–N Voltage THD | Phase 1 voltage total harmonic distortion (THD) |
| L2–L3 Voltage THD | Phase 2 voltage total harmonic distortion (THD) | |
| L3–L1 Voltage THD | Phase 3 voltage total harmonic distortion (THD) |