DOCA0258EN-00

Motor Stop Error Detection

The table lists the motor stop error detection for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0EBE (3775)

83 : 03 : 19

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Function setting

0x0EBF (3776)

83 : 03 : 1A

RW

0.1

s

UINT16

1–60000
(step 1)

10

Y

Time delay

0x0EC0 (3777)

83 : 03 : 1B

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication

3

Y

Reset mode

0x0EC1 (3778)

83 : 03 : 01

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?