LTMT HMI Port Settings
The table lists the HMI port settings for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus/TCP Address (Register) |
EtherNet/IP Address |
RW |
X | Unit |
Type |
Range | Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x112F (4400) |
85 : 02 : 01 |
RW |
1 | – |
UINT16 |
1–247 (step 1) |
1 |
Y |
Node address |
|
0x1130 (4401) |
85 : 02 : 02 |
RW |
1 | – |
UINT16 |
0: None 1: Odd 2: Even |
2 |
Y |
Modbus parity |
|
0x1131 (4402) |
85 : 02 : 03 |
RW |
1 | bps |
UINT16 |
0: 2400 1: 4800 2: 9600 3: 19200 4: 38400 5: 57600 6: 115200 |
3 |
Y |
Baud rate |
|
0x1132 (4403) |
85 : 02 : 04 |
RW |
1 |
– |
UINT16 |
0: Default 1: Programmable |
– |
N |
Control keys |
|
0x1133 (4404) |
85 : 02 : 05 |
RW |
1 |
s |
UINT16 |
1–6000 |
1 |
Y |
Timeout |
|
0x1134 (4405) |
85 : 02 : 06 |
RW | – | – | BITMAP |
0: Big-endian 1: Little-endian |
0 | Y | Byte format |
-
Node address: 1
-
Baud rate: 19200 bps
-
Parity: Even
-
Endianness: Big-endian