LLDP Management Object
Description
The LLDP management object contains the administrative information for the LLDP protocol.
Class Code
The LLDP management object class code is 0x109.
Class Attributes
|
Attribute ID |
Name |
Access |
Description |
|---|---|---|---|
|
0x01 |
Revision |
R |
The LDP management object implementation revision. Returns 0x01. |
|
0x02 |
Maximum instance |
R |
The largest instance number. Returns 0x01. |
|
0x03 |
Number of instances |
R |
The number of object instances. Returns 0x01. |
Class Services
|
Service Code |
Name |
Description |
|---|---|---|
|
0x01 |
Get Attribute All |
Returns the value of all class attributes. |
|
0x0E |
Get Attribute Single |
Returns the value of the specified attribute. |
Instance Attributes
|
Attribute ID |
Name |
Access |
Description |
|---|---|---|---|
|
0x01 |
LDP Enable (LLDP enable array length, LLDP enable array) |
RW |
Number of bits defined in the LLDP enabled array member of the structure |
|
0x02 |
msgTxInterval |
RW |
Interval at which LLDP frames are transmitted from the device* |
|
0x03 |
MsgTxHold |
RW |
Multiplier of msgTxInterval to determine the value of the TTL TLV sent to neighboring devices* |
|
0x04 |
LLDP Datastore |
R |
Indication of the retrieval methods for the LLDP database supported devices |
|
0x05 |
Last Change |
R |
Value of sysUpTime taken the last time any entry in the local LLDP database (ignoring TTL) changed |
Instance Services
|
Service Code |
Name |
Description |
|---|---|---|
|
0x01 |
Get Attribute All |
Returns the value of all class attributes. |
|
0x0E |
Get Attribute Single |
Returns the value of the specified attribute. |
|
0x10 |
Set Attribute Single |
Sets the value of the specified instance attribute. |