DOCA0258EN-00

Phase Over Voltage Protection

The table lists the phase over voltage protection for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0E31 (3634)

83 : 02 : 09

RW

1

UINT16

  • 0 - Disable

  • 1 - Alarm
  • 2 - Trip
  • 3 - Alarm and Trip

2

Y

Function setting

0x0E32 (3635)

83 : 02 : 0A

RW

1

%Vn

UINT16

101–130
(step 1)

110

Y

Pickup

0x0E33 (3636)

83 : 02 : 0B

RW

0.1

s

UINT16

1–60000
(step 1)

50

Y

Time delay

0x0E34 (3637)

83 : 02 : 0C

RW

1

%Vn

UINT16

101–130
(step 1)

110

Y

Alarm level

0x0E35 (3638)

83 : 02 : 0D

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0E36 (3639)

83 : 02 : 0E

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0E37 (3640)

83 : 02 : 0F

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?