DOCA0258EN-00

Communication Loss

The table lists the communication loss for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0EC8 (3785)

83 : 03 : 23

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

0

Y

Function setting

0x0EC9 (3786)

83 : 03 : 24

RW

0.1

s

UINT16

1–60000
(step 1)

10

Y

Time delay

0x0ECA (3787)

83 : 03 : 25

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0ECB (3788)

83 : 03 : 26

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0ECC (3789)

83 : 03 : 27

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Trip only in remote mode

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?