DOCA0258EN-00

Daylight Saving Settings

The table lists the Daylight Saving Settings for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X Unit

Type

Range Default value

Svd

Description

0x13D1 (5074)

88 : 01 : C7

RW

1

N/A

UINT16

0: Disable

1: Enable

0

Y

Daylight Saving Selection

0x13D2 (5075)

88 : 01 : C8

RW

1

N/A

UINT16

1–5
(step 1)

1

Y

Start Day

0x13D3 (5076)

88 : 01 : C9

RW

1

N/A

UINT16

1: Sunday

2: Monday

3: Tuesday

4: Wednesday

5: Thursday

6: Friday

7: Saturday

1

Y

Start Week

0x13D4 (5077)

88 : 01 : CA

RW

1

N/A

UINT16

1–12
(step 1)

1

Y

Start Month

0x13D5 (5078)

88 : 01 : CB

RW

1

N/A

UINT16

0–23
(step 1)

0

Y

Start Time

0x13D6 (5079)

88 : 01 : CC

RW

1

N/A

UINT16

1–5
(step 1)

1

Y

End Day

0x13D7 (5080)

88 : 01 : CD

RW

1

N/A

UINT16

1: Sunday

2: Monday

3: Tuesday

4: Wednesday

5: Thursday

6: Friday

7: Saturday

1

Y

End Week

0x13D8 (5081)

88 : 01 : CE

RW

1

N/A

UINT16

1–12
(step 1)

1

Y

End Month

0x13D9 (5082)

88 : 01 : CF

RW

1

N/A

UINT16

0–23
(step 1)

0

Y

End Time

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?