Under Power Factor Protection
The table lists the under power factor protection for the The table lists the over power protection for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0E65 (3686) |
83 : 02 : 3D |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0E66 (3687) |
83 : 02 : 3E |
RW |
0.10 |
PF |
UINT16 |
40–100 |
60 |
Y |
Pickup |
|
0x0E67 (3688) |
83 : 02 : 3F |
RW |
0.1 |
s |
UINT16 |
1–60000 |
1 |
Y |
Time delay |
|
0x0E68 (3689) |
83 : 02 : 40 |
RW |
0.10 |
PF |
UINT16 |
40–100 |
60 |
Y |
Alarm level |
|
0x0E69 (3690) |
83 : 02 : 41 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0E6A (3691) |
83 : 02 : 42 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0E6B (3692) |
83 : 02 : 43 |
– |
– |
– |
– |
– |
– |
– |
Reserved |