Motor Run Indicators
The table lists the motor run indicators for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|
|
0x0210 (529) |
R |
BOOL | N |
Motor forward running |
|
0x0211 (530) |
R |
BOOL | N |
Motor reverse running |
|
0x0212 (531) |
R |
BOOL | N |
Motor fast forward running |
|
0x0213 (532) |
R |
BOOL | N |
Motor fast reverse running |
|
0x0214 (533) |
R |
BOOL | N |
Motor running in star (forward) |
|
0x0215 (534) |
R |
BOOL | N |
Motor running in delta (forward) |
|
0x0216 (535) |
R |
BOOL | N |
Motor running in star (reverse) |
|
0x0217 (536) |
R |
BOOL | N |
Motor running in delta (reverse) |
|
0x0218 (537) |
R |
BOOL | N |
Motor in star-delta changeover (forward) |
|
0x0219 (538) |
R |
BOOL | N |
Motor in star-delta changeover (reverse) |
|
0x021A (539) |
R |
BOOL | N |
Interlocking time active |
|
0x021B (540) |
R |
BOOL | N |
Change-over pause active |
|
0x021C–0x021F (541–544) |
– |
– |
– |
Reserved |