DOCA0258EN-00

Normal Inverse Overcurrent Protection

The table lists the normal inverse overcurrent protection for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0DD2 (3539)

83 : 01 : 27

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

0

Y

Function setting

0x0DD3 (3540)

83 : 01 : 28

RW

1

%IFLC

UINT16

20–1000
(step 1)

50

Y

Pickup

0x0DD4 (3541)

83 : 01 : 29

RW

0.1

s

UINT16

1–200
(step 1)

1

Y

Time delay (TMS)

0x0DD5 (3542)

83 : 01 : 2A

RW

1

%IFLC

UINT16

20–1000
(step 1)

50

Y

Alarm level

0x0DD6 (3543)

83 : 01 : 2B

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0DD7 (3544)

83 : 01 : 2C

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0DD8 (3545)

83 : 01 : 2D

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?