DOCA0258EN-00

Connection to the Network

Every LTMT main unit includes an embedded two-port Ethernet switch with one IP address.

NOTE: The LTMT main unit includes an internal two-port bridge. Both RJ45 ports share one IP address. Use only star or point-to-point topologies.

The IEEE 802.3 standard defines EthernetLTMT main unit

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?