DOCA0258EN-00

LTMT Main Unit Device Internal Error Detection Setting

The table lists the different device internal error detection setting of LTMT main unit.

Modbus TCP/IP Address (Register)

RW

Type

Svd

Description

0x0260 (609)

R

BOOL N

Sensor module communication error detected

0x0261 (610)

R

BOOL N

LTMT expansion module communication error detected

0x0262 (611)

R

BOOL N

HMI communication error detected

0x0263 (612)

R

BOOL N

EEPROM interface error detected

0x0264 (613)

R

BOOL N

EEPROM checksum error detected

0x0265 (614)

R

BOOL N

Configuration error detected

0x0266–0x0267 (616–615)

R

BOOL N

Reserved

0x0268 (617)

R

BOOL N

Watchdog timeout detected

0x0269–0x026B (618–620)

R

BOOL N

Reserved

0x026C (621)

R

BOOL N

Energy register overflow

0x026D (622)

R

BOOL N

Error detected during LTMT expansion module initialization

0x026FE–0x027F (623–640)

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?