Permissive Commands Status
The table lists the permissive commands status for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|
| 0x0220 (545) |
R |
BOOL | N |
Status - Permissive Command 1 |
| 0x0221 (546) |
R |
BOOL | N |
Status - Permissive Command 2 |
| 0x0222 (547) |
R |
BOOL | N |
Status - Permissive Command 3 |
| 0x0223 (548) |
R |
BOOL | N |
Status - Permissive Command 4 |
| 0x0224 (549) |
R |
BOOL | N |
Status - Permissive Command 5 |
| 0x0225 (550) |
R |
BOOL | N |
Status - Permissive Command 6 |
| 0x0226 (551) |
R |
BOOL | N |
Status - Permissive Command 7 |
| 0x0227 (552) |
R |
BOOL | N |
Status - Permissive Command 8 |
| 0x0228–0x023F (553–576) |
– |
– |
– |
Reserved |