Motor Status
The table lists the motor status for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|
|
0x00F0 (241) |
R |
BOOL | N |
Motor Stop |
|
0x00F1 (242) |
R |
BOOL | N |
Motor Start |
|
0x00F2 (243) |
R |
BOOL | N |
Motor Run |
|
0x00F3 (244) |
R |
BOOL | N |
Motor Inhibit |
| 0x00F4 (245) |
R |
BOOL | N | Remote Mode |
|
0x00F5–0x00FF (246–256) |
– |
– |
– |
Reserved |