DOCA0258EN-00

Monitoring Page Body

The Monitoring page contains the following read-only data:

Level 1 Level 2 Parameter Name
Motor Status* Starter Type

Starter type. Possible values:

  • Direct online

  • Reversible Direct Online

  • Star Delta

  • Overload

  • Heater

Load Status

Load status. Possible values:

  • Stop

  • Start

  • Run

Motor Control*

Motor control. Possible values:

  • Start

  • Stop

Motor Data Motor Status

Motor status. Possible values:

  • Stop

  • Start

  • Run

  • Trip

  • Inhibit

  • Forward start & Run

  • Reverse Start & Run

Max Starts Counter Maximum starts counter
Max Start Inhibit Time Maximum start inhibit time
Motor Starting Peak Current Motor starting peak current
Motor Starting Time Motor starting time
Total Run Hour Total run hour
Last Run Hour Last run hour
Number of Starts Number of starts
Number of Stops Number of stops
Motor Stop Cause

Motor stop cause. Possible values:

  • None

  • HMI

  • Local DI

  • Remote DI

  • Communication

  • Auto restart

  • Trip

  • No current

  • Force stop

  • Direction change

  • No feedback

  • Speed change

  • Custom stop

  • Mode transfer

  • Device internal

  • No voltage

  • Voltage dip

Active Trip Counter Active trip counter
Thermal Memory Thermal memory
Thermal Time to Trip Thermal time to trip
Thermal Time to Cool Thermal time to cool
Inhibit Status No Voltage Inhibit No voltage inhibit
Under Voltage Inhibit Under voltage inhibit
Trip Inhibit Trip Inhibit
Thermal Inhibit Thermal Inhibit
Max Starts Inhibit Maximum starts inhibit
Interlock 1 Inhibit Interlock 1 Inhibit
Interlock 2 Inhibit Interlock 2 Inhibit
Interlock 3 Inhibit Interlock 3 Inhibit
Interlock 4 Inhibit Interlock 4 Inhibit
Interlock 5 Inhibit Interlock 5 Inhibit
Interlock 6 Inhibit Interlock 6 Inhibit
Interlock 7 Inhibit Interlock 7 Inhibit
Interlock 8 Inhibit Interlock 8 Inhibit
Interlock 9 Inhibit Interlock 9 Inhibit
Interlock 10 Inhibit Interlock 10 Inhibit
Interlock 11 Inhibit Interlock 11 Inhibit
Interlock 12 Inhibit Interlock 12 Inhibit
Local DI Stop Inhibit Local DI Stop Inhibit
Remote DI Stop Inhibit Remote DI Stop Inhibit
Communication Stop Inhibit Communication Stop Inhibit
Force Stop Inhibit Force Stop Inhibit
Antibackspin Inhibit Antibackspin Inhibit
Direction Change Inhibit Direction Change Inhibit
Custom Stop Inhibit Custom Stop Inhibit
Firmware Update Inhibit Firmware Update Inhibit

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?