DOCA0258EN-00

Change Password

Overview

The Change Password feature allows you to update the account credentials securely. This helps maintain account security and ensures that only authorized users can access the standard web server. 

Change Your Password

To change your password in the standard web server, proceed as follows.

  1. Navigate to Administrator > Change Password in the top-right corner of the screen.

    Result: The Change Password dialog box appears.

  2. Provide the following information and click Submit:

    • Current Password

    • New Password

    • Confirm Password

    NOTE: To ensure account security, your new password must:
    • Be at least eight characters long.

    • Include at least one uppercase and lowercase letters from a to z.

    • Contain at least one number from 0 to 9.

    • Include at least one special character (example: !, @, &, * and so on).

    • Avoid using three or more consecutive identical or sequential characters (example: aaa, 111, 123, and so on).

    • Avoid using most common passwords.

    Result: The Password Modified Successfully message appears.

  3. Click OK.

    Result: You are redirected to the login page.

  4. Enter Administrator in the Username field and your new password in the Password field.

  5. Click Login.

    Result: The Monitoring & Control page appears.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?