DOCA0258EN-00

Communication Status

The table lists the communication status for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

RW

Type

Svd

Description

0x02A0 (673)

R

BOOL N

Modbus RTU port: No communication

0x02A1 (674)

R

BOOL N

HMI port: No communication

0x02A2–0x02BF (675–704)

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?