DOCA0258EN-00

Current Phase Reversal Protection

The table lists the current phase reversal protection for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0E02 (3587)

83 : 01 : 57

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

2

Y

Function setting

0x0E03 (3588)

83 : 01 : 58

RW

0.1

s

UINT16

1–60000
(step 1)

1

Y

Time delay

0x0E04 (3589)

83 : 01 : 59

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0E05 (3590)

83 : 01 : 5A

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0E06 (3591)

83 : 01 : 5B

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?