DOCA0258EN-00

Anti-Backspin Timer

The table lists the anti-backspin timer for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0EDA (3803)

83 : 03 : 35

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Function setting

0x0EDB (3804)

83 : 03 : 36

RW

1

s

UINT16

0–60000
(step 1)

0

Y

Time delay

0x0EDC (3805)

83 : 03 : 37

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?