DOCA0258EN-00

Connection Manager Object

Description

The connection manager object establishes and manages the run-time exchange of messages between devices.

Class Code

The connection manager object class code is 0x06 as defined by CIP.

Class Attributes

Attribute ID

Name

Access

Description

0x01

Revision

R

The Connection Manager implementation revision.

Returns 0x01.

0x02

Maximum Instance

R

The largest instance number.

Returns 0x01.

0x03

Number of Instances

R

The number of object instances.

Returns 0x01.

Class Services

Service Code

Name

Description

0x01

Get Attribute All

Returns the value of all class attributes.

0x0E

Get Attribute Single

Returns the value of the specified attribute.

Instance Codes

Only one instance is implemented: Instance 1.

Instance Attributes

Attribute ID

Name

Access

Description

0x01

Incoming Forward Open requests count

RW

Total number of incoming connection open requests.

0x02

Forward Open Format Unsuccessful count

RW

The number of Forward Open requests rejected because of the unexpected format of the Forward Open request.

0x03

Forward Open Resource Unsuccessful count

RW

The number of Forward Open requests rejected because of insufficient resources.

0x04

Forward Open Parameter Value count

RW

The number of Forward Open requests rejected because of the parameter value sent with Forward Open.

0x05

Incoming Forward Close requests count

RW

Total number of incoming connection close requests.

0x06

Forward Close Format Unsuccessful count

RW

The number of Forward Close requests that has invalid format.

0x07

Forward Close Matching Unsuccessful count

RW

The number of Forward Close requests that could not be matched to an active connection.

0x08

Timed out Connections count

RW

The number of connections that has timed out because the other side stopped producing or there was a network interruption.

Instance Services

Service Code

Name

Description

0x01

Get Attribute All

Returns the value of all instance attributes.

0x0E

Get Attribute Single

Returns the value of the specified instance attribute.

0x4E

Forward Close

Closes an existing connection.

0x54

Forward Open

Opens a new connection.

0x5B

Large Forward Open

Opens a new connection with maximum size buffer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?