DOCA0258EN-00

Phase Under Voltage Protection

The table lists the phase under voltage protection for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0E29 (3626)

83 : 02 : 01

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

2

Y

Function setting

0x0E2A (3627)

83 : 02 : 02

RW

1

%Vn

UINT16

20–100
(step 1)

80

Y

Pickup

0x0E2B (3628)

83 : 02 : 03

RW

0.1

s

UINT16

1–60000
(step 1)

100

Y

Time delay

0x0E2C (3629)

83 : 02 : 04

RW

1

%Vn

UINT16

20–100
(step 1)

80

Y

Alarm level

0x0E2D (3630)

83 : 02 : 05

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

8

Y

Reset mode

0x0E2E (3631)

83 : 02 : 06

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0E2F (3632)

83 : 02 : 07

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?