DOCA0258EN-00

User Map Data for Registers

The user map data are designed to optimize the access to 100 non-contiguous registers maximum in one single request. You can define several read and write areas.

The user map can be defined through:

  • PC running the TeSys Tera DTM Library embedded in a FDT container like SoMove software

  • PLC or DCS through the communication network

User Map Addresses

The user map addresses are used to select a list of addresses to read or write. It can be considered as a configuration area.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

Type

Range

Svd

Description

0x0320 (801)

6D : 01 : 01

RW

UINT16

1-9249

Y

User map address 1

0x0321 (802)

6D : 01 : 02

RW

UINT16

1-9249

Y

User map address 2

0x0322 (803)

6D : 01 : 03

RW

UINT16

1-9249

Y

User map address 3

0x0383 (900)

6D : 01 : 64

RW

UINT16

1-9249

Y

User map address 100

User Map Values

The user map values are used to read or write values associated to addresses configured in the user map addresses.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

Type

Range

Svd

Description

0x0384 (901)

6E : 01 : 01

RW

UINT16

1-65535

N

User map value 1

0x0385 (902)

6E : 01 : 02

RW

UINT16

1-65535

N

User map value 2

0x0386 (903)

6E : 01 : 03

RW

UINT16

1-65535

N

User map value 3

0x03E7 (1000)

6E : 01 : 64

RW

UINT16

1-65535

N

User map value 100

Read or write of address 0x0384 or register 901 allows to read or write the value in address defined in address 0x0320 or register 801.

Read or write of address 0x0385 or register 902 allows to read or write the value in address defined in address 0x0321 or register 802, and so on.

Example

The following table gives an example of user map address configuration to access non-contiguous registers:

Modbus TCP/IP Address (Register)

EtherNet/IP Address

Modbus TCP/IP Address configured

Description

0x0320 (801)

6D : 01 : 01

0x15B5

Motor status

0x0321 (802)

6D : 01 : 02

0x15C8

Motor stop cause

0x0322 (803)

6D : 01 : 03

0x160D

Trip status MSW

0x0323 (804)

6D : 01 : 04

0x160E

Trip status LSW

0x0324 (805)

6D : 01 : 05

0x15B6

Thermal memory

0x0325 (806)

6D : 01 : 06

0x1586

Average current (0.001 A) MSW

0x0326 (807)

6D : 01 : 07

0x1587

Average current (0.001 A) LSW

0x0352 (851)

6D : 01 : 33

0x02C0

Control register 1

0x0353 (852)

6D : 01 : 34

0x02C1

Control register 2

With this configuration, monitoring information is accessible with one single read request through addresses 0x0384 to 0x038A or registers 901 to 907.

Configuration and command can be written with one single write using addresses 0x03B6 to 0x03B7 or registers 951 to 952.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?