DOCA0258EN-00

Starter Commands

The table lists the starter commands for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

RW

Type

Svd

Description

0x01F0 (497)

R

BOOL N

CONTACTOR OUTPUT 1

0x01F1 (498)

R

BOOL N

CONTACTOR OUTPUT 2

0x01F2 (499)

R

BOOL N

CONTACTOR OUTPUT 3

0x01F3 (500)

R

BOOL N

CONTACTOR OUTPUT 4

0x01F4 (501)

R

BOOL N

CONTACTOR OUTPUT 5

0x01F5–0x020E (502–527)

Reserved

0x020F (528)

R

BOOL N Motor Stop
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?