Over Power Protection
The table lists the over power protection for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0E5E (3679) |
83 : 02 : 36 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0E5F (3680) |
83 : 02 : 37 |
RW |
1 |
%P * |
UINT16 |
20–1000 |
110 |
Y |
Pickup |
|
0x0E60 (3681) |
83 : 02 : 38 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
1 |
Y |
Time delay |
|
0x0E61 (3682) |
83 : 02 : 39 |
RW |
1 |
%P * |
UINT16 |
20–1000 |
110 |
Y |
Alarm level |
|
0x0E62 (3683) |
83 : 02 : 3A |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0E63 (3684) |
83 : 02 : 3B |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0E64 (3685) |
83 : 02 : 3C |
– |
– |
– |
– |
– |
– |
– |
Reserved |