Modbus RTU Diagnostics
The table lists the Modbus RTU diagnostics for the Modbus TCP/IP communication.
|
Modbus TCP/IP Address (Register) |
RW |
X | Unit | Range | Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|
|
0xA85A (43099) |
R |
1 |
– |
0–4294967295 |
– |
– |
Frames Received |
|
0xA85C (43101) |
R |
1 |
– |
0–4294967295 |
– |
– |
Frames Transmitted |
|
0xA85E (43103) |
R |
1 |
– |
0: 2400 1: 4800 2: 9600 3: 19200 4: 38400 5: 57600 6: 115200 |
– |
– |
Baud rate |
|
0xA85F (43104) |
R |
1 |
– |
0: None 1: Odd 2: Even |
– |
– |
Parity |
|
0xA860 (43105) |
R |
1 |
– |
0: 0 1: 1 2: 2 |
– |
– |
Stop Bit |
|
0xA861 (43106) |
R |
1 |
– |
1–247 |
– |
– |
Server ID |