DOCA0258EN-00

Motor Start Logs

Description

The LTMT main unit records 250 current values measured during the last motor start.

One log can be saved to serve as motor start reference log.

The last motor start log can be saved as reference log by using:

  • The TeSys Tera DTM.

  • A command from a PLC or DCS through the communication network.

The last motor start log and the reference log:

  • Can be displayed with the TeSys Tera DTM.

  • Are available for PLC or DCS through the communication network.

Two read requests of 128 registers are necessary to read the last motor start log, and two read requests of 128 registers are necessary to read the reference log.

Sampling Interval

The sampling interval is based on the trip class selected in the thermal overload settings.
Trip class Sampling interval
5 20 ms
10 40 ms
15 60 ms
20 80 ms
25 100 ms
30 120 ms
35 140 ms
40 160 ms

Last Motor Start Log Registers

The table lists the registers for the last motor start log.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range Default value

Svd

Description

0x20B7 (8376)

82 : 8D : 01

R

UINT16

Y Date and Time

Reference Log Registers

The table lists the registers for the reference log.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range Default value

Svd

Description

0x222E (8751)

82 : 8E : 01

R

UINT16

Y Date and Time
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?