Expansion Module Details Page Body
The Expansion Module Details page contains the following sub-menus:
| Level 1 | Level 2 | Parameter Name |
|---|---|---|
| Expansion Module - 1 (4DI2DO) | Digital Input 5 | Digital input |
| Digital Input 6 | Digital input | |
| Digital Input 7 | Digital input | |
| Digital Input 8 | Digital input | |
| Digital Output 4 | Digital output | |
| Digital Output 5 | Digital output | |
| Expansion Module - 2 (4DI2DO) | Digital Input 9 | Digital input |
| Digital Input 10 | Digital input | |
| Digital Input 11 | Digital input | |
| Digital Input 12 | Digital input | |
| Digital Output 6 | Digital output | |
| Digital Output 7 | Digital output | |
| Expansion Module - 3 (4DI2DO) | Digital Input 13 | Digital input |
| Digital Input 14 | Digital input | |
| Digital Input 15 | Digital input | |
| Digital Input 16 | Digital input | |
| Digital Output 8 | Digital output | |
| Digital Output 9 | Digital output | |
| Expansion Module - 4 (4DI2DO) | Digital Input 17 | Digital input |
| Digital Input 18 | Digital input | |
| Digital Input 19 | Digital input | |
| Digital Input 20 | Digital input | |
| Digital Output 10 | Digital output | |
| Digital Output 11 | Digital output | |
| Expansion Module - 5 (4DI2DO) | Digital Input 21 | Digital input |
| Digital Input 22 | Digital input | |
| Digital Input 23 | Digital input | |
| Digital Input 24 | Digital input | |
| Digital Output 12 | Digital output | |
| Digital Output 13 | Digital output |