DOCA0258EN-00

Device Internal

The table lists the device internal setting for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0EC3 (3780)

83 : 03 : 1E

RW

1

UINT16

  • 0: Disable

  • 1: Enable

1

Y

Function setting

0x0EC4 (3781)

83 : 03 : 1F

RW

0.1

Seconds

UINT16

10

Y

Time delay

0x0EC5 (3782)

83 : 03 : 20

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication

3

Y

Reset mode

0x0EC6–0x0EC7 (3783–3784)

83 : 03 : 21– 83 : 03 : 22

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?