DOCA0258EN-00

Time Zone Settings Page Body

The Time Zone settings page contains the following sub-menus:

Level 1 Level 2 Parameter Name
Time Zone Time Zone Offset Time Zone Offset. Use the toggle key to enable or disable the feature.
Daylight Saving Enable Daylight Saving Enable
Daylight Saving Time Begins Daylight Saving Time Begins
Daylight Saving Time Ends Daylight Saving Time Ends
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?